Reliability Automation Rule Data Model

The following diagram shows how the families used in Reliability Automation Rules are related to one another.



Note: In the diagram, boxes represent entity families and arrows represent relationship families that are configured in the baseline database. You can determine the direction of the each relationship definition from the direction of the arrow head: the box from which the arrow originates is the predecessor, and the box to which the arrow head points is the successor.