Install the GE Digital APM Mobile Application on a Windows Device
Procedure
- Access the application package file at C:\Program Files\Meridium\ApplicationServer\distribution\GEDigitalAPM.zip.Note:
- Access the application package file at C:\Program Files\Meridium\ApplicationServer\distribution\GEDigitalAPM.zip.Note:
- On the device on which you want to install the GE Digital APM mobile application, extract the content of the application package file to a local folder.
- In the folder into which you extracted the application package file content, right-click Install.bat, and then select Run as an Administrator.Note: If you are using a touch-screen device, press and hold Install.bat, and then select Run as an Administrator.The GE Digital APM mobile application is installed on the Windows device for all current and future Windows user accounts.
- Optional: To cancel future installations or uninstall the GE Digital APM mobile application, in the folder into which you extracted the application package file content, right-click Uninstall.bat, and then select Run as an Administrator.Note: If you are using a touch-screen device, press and hold Uninstall.bat, and then select Run as an Administrator.The GE Digital APM mobile application is uninstalled for the Windows user account that is currently logged in, and installations for future Windows user accounts are canceled.