Entities Overview in Change Management
There are two types of Change Management projects.
- CIMPLICITY project.
- Computer project.
There are two classes of entities that can be added to Change Management for each project type.
Entity Class | Description |
---|---|
Base Configuration | A collection of interrelated files that must remain interrelated and, thus, must be managed as a single unit. |
Individually managed files | Files that can be managed as individual units. |

Field | Description | |
---|---|---|
CIMPLICITY Project | ||
Project |
All user configurable configuration files in the CIMPLICITY project can be added to Change Management.
Project configuration includes:
|
|
Base Configuration |
Files that make up the project's basic configuration, e.g. points, alarms, configuration files, are required for the project processes to run.
Note: The processes start when the project starts.
Base configuration files:
Important: Base configuration must be added once to be managed.
|
|
Individually managed files |
Single files that are listed in the CIMPLICITY project’s Managed files folder can be added separately to Change Management. These files, e.g. CimView screens and scripts, are individually controlled.
Individually managed files:
![]() |
|
Computer Project | ||
Computer |
All files in the computer project can be added to Changed Management.
Computer files include:
|
|
Base Configuration | Files included in the system's basic configuration, e.g. globals.ini, cimhosts.txt. These files are required for the Computer project system's processes to run. | |
Managed files | Single files that are listed in the Computer project’s Managed files folder can be added separately to Change Management. These files are individually controlled and are not required for the Computer project's processes to run. These files, e.g. CimView screens and scripts, are individually controlled. Individually managed files:
![]() |