Marquee Manager Administrator Tools: Users
If Windows or Windows Trusted is selected for the server security, a Users folder is added to the Tools tree, if it was not already there.
Important:
- Security is configured separately in the Marquee Manager components:
- Marquee Manager Administrator
- Marquee Gateway
- Marquee Manager Client authenticates against configured Marquee Manager Administrator users when Security is enabled.
- New User
- Details Tab
New User
Do the following.

A | Select Users in the Marquee Manager Administrator window left-pane. |
B | Click New User on the Marquee Manager Administrator window toolbar. |
Result: Tabs for the User profile display in the Alarm Cast Administrator right-pane.
Details Tab
Details options to register Marquee Manager users are as follows.

Field | Description | ||
---|---|---|---|
User | |||
Username | Valid Windows user. | ||
Domain | Domain the user logs into. | ||
Password | (Required with Windows Security) Password assigned to the logged in Windows user. | ||
Confirm | (Required with Windows Security) Re-entered password. | ||
Security | Security levels are as follows. | ||
ADMIN |
Full rights to all features.
Important: The ADMIN security level is required to access (open) applications. For almost all instances, it is recommended that ADMIN be assigned to registered Marquee Manager users.
|
||
USER | Can access only the Marquee Manager Client. | ||
DEFAULT | USER | ||
Notes | |||
Notes | (Optional) Additional details about or for the user. |