Alarm Categories for an OPC Alarm and Event Server
These are the categories of CIMPLICITY alarm messages that passed as OPC alarm messages:
Category | Used for |
---|---|
Level | Non-Boolean point alarms Text messages come from the alarm strings definition used by the alarm. |
Discrete | Boolean point alarms Text messages come from the alarm strings definition used by the alarm. |
System | All non-point alarms Non-point alarms have a configurable severity. This severity is used by the OPC server as the sub-condition System severity.Note: Existing non-point alarms have a default severity of 100. |