About the Basic Control Syntax
This section contains a complete, alphabetical listing of all keywords in the Basic Control Engine script language. When syntax is described, the following notations are used:
Notation | Description | ||
While...Wend | Elements belonging to the Basic Control Engine script language, referred to in this manual as keywords, appear in the typeface shown to the left. | ||
variable | Items that are to be replaced with information that you supply appear in italics. The type of replacement is indicated in the following description. | ||
text$ | The presence of a type-declaration character following a parameter signifies that the parameter must be a variable of that type or an expression that evaluates to that type. If a parameter does not appear with a type-declaration character, then its type is described in the text. | ||
[parameter] | Square brackets indicate that the enclosed items are optional. In Basic Control Engine script language, you cannot end a statement with a comma, even if the parameters are optional: | ||
|
|
||
|
|
||
{Input | Binary} | Braces indicate that you must choose one of the enclosed items, which are separated by a vertical bar. | ||
... | Ellipses indicate that the preceding expression can be repeated any number of times. |