Syntax
|
AlarmUpdate Project$, AlarmId$, ResourceId$, Action% ,caObj
[, AlarmMessage$ [, UserId$ [,RefId$]]]
|
Description
|
To update a currently generated Change approval alarm.
The alarm being updated may be of any alarm type. However, if the AlarmMessage$ is specified, it must be an alarm with an alarm type of $CIMBASIC .
|
Comments
|
Parameter
|
Description
|
|
Project$
|
String. The project to generate the alarm on, an empty string "" indicates the current project
|
|
AlarmId$
|
String. The ID of the Alarm. Must be a valid alarm.
|
|
ResourceId$
|
String. The Resource ID to generate the alarm against. Used to control routing of the alarm.
|
|
Action%
|
Integer. Indicates whether to acknowledge or reset the alarm. Use the manifest constants AM_ACKNOWLEDGED and AM_RESET to perform an acknowledgment and a reset.
By default, on a computer with Server Redundancy, alarm updates from the slave computer's Event Manager are ignored. To acknowledge or reset an alarm on the master computer from the slave computer, use AM_ACKNOWLEDGED_M or AM_RESET_M to override the default behavior.
|
|
caObj
|
Object of type CimAlmChangeApprovalData . It contains Change Approval information.
|
|
AlarmMessage$
|
String. (optional). The update alarm message to display.
Note: This string is substituted into the first variable field of the Alarm's message. For a user-defined alarm message, this will be the first %s field in the message. For a point alarm message, it will be the first variable field (%VAL , %ID , etc.) in the alarm message. For this reason, it is not recommended that you use the AlarmMessage$ field when updating point alarms.
|
|
UserId$
|
String. (optional). The User ID which generated the alarm.
|
|
RefId$
|
String. A Reference ID used to distinguish between identical alarms. The Reference ID needs to match the Reference ID of the generated alarm. If the alarm was generated without a Reference ID, then this field can be omitted from the call.
|
Example
|
sub main()
Dim obj As New CimAlmChangeApprovalData
obj.PerformerUserid = "OPERATOR"
obj.PerformerPassword = ""
obj.PerformerComment= "bool=1 from BCE"
obj.VerifierUserid = "MANAGER"
obj.VerifierPassword = ""
obj.VerifierComment= "bool=1 from BCE"
AlarmUpdateCA "ESIGDEMO","CA_TESTPOINT","$MAC_FR",AM_ACKNOWLEDGED,CAobj, "CA_TESTPOINT","CA_TESTPOINT","CA_TESTPOINT"
end sub
|
See Also
|
AlarmGenerate (method)
|
Note
|
When updating an alarm, the AlarmId$, ResourceId$ and RefId$ must match exactly to the alarm to be updated; if they do not match the alarm will not be updated.
When updating a point alarm, the RefId$ is always the Point ID (which is also the Alarm ID).
|