AlarmUpdate (method)
Syntax | AlarmUpdate Project$, AlarmId$ , ResourceId$ , Action% [ , AlarmMessage$ [ , UserId$ [ , RefId$]]] | |
Description | To update a currently generated alarm. The alarm being updated may be of any alarm type. However, if the AlarmMessage$ is specified, it must be an alarm with an alarm type of $CIMBASIC. | |
Comments | Parameter | Description |
Project$ | String. The project to generate the alarm on, an empty string "" indicates the current project | |
AlarmId$ | String. The ID of the Alarm. Must be a valid alarm. | |
ResourceId$ | String. The Resource ID to generate the alarm against. Used to control routing of the alarm. | |
Action% |
Integer. Indicates whether to acknowledge or reset the alarm. Use the manifest constants AM_ACKNOWLEDGED and AM_RESET to perform an acknowledgment and a reset.
By default, on a computer with Server Redundancy, alarm updates from the slave computer's Event Manager are ignored. To acknowledge or reset an alarm on the master computer from the slave computer, use
AM_ACKNOWLEDGED_M
or
AM_RESET_M
to override the default behavior.
|
|
AlarmMessage$ |
String. (optional). The update alarm message to display.
Note: This string is substituted into the first variable field of the Alarm's message. For a user-defined alarm message, this will be the first
%s
field in the message. For a point alarm message, it will be the first variable field (%VAL , %ID , etc.) in the alarm message. For this reason, it is not recommended that you use the AlarmMessage$ field when updating point alarms.
|
|
UserId$ | String. (optional). The User ID which generated the alarm. | |
RefId$ | String. A Reference ID used to distinguish between identical alarms. The Reference ID needs to match the Reference ID of the generated alarm. If the alarm was generated without a Reference ID, then this field can be omitted from the call. | |
Example |
|
|
See Also | AlarmGenerate (method) | |
Note | When updating an alarm, the AlarmId$, ResourceId$ and RefId$ must match exactly to the alarm to be updated; if they do not match, the alarm will not be updated. When updating a point alarm, the RefId$ is always the Point ID (which is also the Alarm ID). Guidelines that apply to |