Syntax
|
AppMaximize
[name$]
|
Description
|
Maximizes the named application.
|
Comments
|
The name$ parameter is a
String
containing the name of the desired application. If it is omitted, then the
AppMaximize
function maximizes the active application.
|
Example
|
Sub Main()
AppMaximize "Program Manager" 'Maximize Program Manager.
If AppFind$("NotePad") <> "" Then
AppActivate "NotePad" 'Set the focus to NotePad.
AppMaximize 'Maximize it.
End If
End Sub
|
See Also
|
AppMinimize (statement); AppRestore (statement); AppMove (statement); AppSize (statement); AppClose (statement).
|
Notes
|
If the named application is maximized or hidden, the
AppMaximize
statement will have no effect.
The name$ parameter is the exact string appearing in the title bar of the named application's main window. If no application is found whose title exactly matches name$, then a second search is performed for applications whose title string begins with name$. If more than one application is found that matches name$, then the first application encountered is used.
AppMaximize
generates a runtime error if the named application is not enabled, as is the case if that application is displaying a modal dialog box.
|