Syntax
|
Basic.Processor$
|
Description
|
Returns a String containing the name of the CPU in the computer on which BasicScript is running.
|
Comments
|
Sample values returned for Win32 platforms include:
|
|
Platform
|
Sample Value returned
|
|
Intel
|
80386
80486
Pentium
|
|
MIPS
|
The string "Rx" such as R4000
|
|
Alpha
|
321064
321066
321164
|
|
PowerPC
|
601
603
604
603+
604+
620
|
Example
|
'
'This example prints the CPU of the computer on which
'BasicScript is executing.
'
Sub Main()
MsgBox "Processor = " & Basic.Processor$
End Sub
|
See Also
|
Basic.ProcessorCount (property)
|
Note
|
You can retrieve the number of processors within the computer using the Basic.ProcessorCount property.
|