DlgEnable (statement)
Syntax | DlgEnable {ControlName$ | ControlIndex} [,isOn] |
Description | Enables or disables the specified control. |
Comments | Disabled controls are dimmed and cannot receive keyboard or mouse input. The isOn parameter is an Integer specifying the new state of the control. It can be any of the following values: 0 The control is disabled. 1 The control is enabled. Omitted Toggles the control between enabled and disabled. |
Option buttons can be manipulated individually (by specifying an individual option button) or as a group (by specifying the name of the option group). | |
The ControlName$ parameter contains the name of the .Identifier parameter associated with a control in the dialog box template. Alternatively, by specifying the ControlIndex parameter, a control can be referred to using its index in the dialog box template (0 is the first control in the template, 1 is the second, and so on). | |
Example |
This example uses DlgEnable to turn on/off various dialog options.
|
|
|
See Also | DlgEnable (function); DlgFocus (function); DlgFocus (statement); DlgListBoxArray (function); DlgListBoxArray (statement); DlgSetPicture (statement); DlgText (statement); DlgText$ (function); DlgValue (function); DlgValue (statement); DlgVisible (statement); DlgVisible (function). |