Syntax
|
DlgValue
{ControlName$ | ControlIndex},Value
|
Description
|
Changes the value of the given control.
|
Comments
|
The value of any given control is an
Integer
and depends on its type, according to the following table:
|
|
Control Type
|
Description of Value
|
|
Option group
|
The index of the new selected option button within the group (0 is the first option button, 1 is the second, and so on).
|
|
List box
|
The index of the new selected item.
|
|
Drop list box
|
The index of the new selected item.
|
|
Check box
|
1 if the check box is to be checked; 0 if the check is to be removed.
|
|
A runtime error is generated if
DlgValue
is used with controls other than those listed in the above table.
|
|
The ControlName$ parameter contains the name of the .Identifier parameter associated with a control in the dialog box template. A case-insensitive comparison is used to locate the specific control within the template. Alternatively, by specifying the ControlIndex parameter, a control can be referred to using its index in the dialog box template (0 is the first control in the template, 1 is the second, and so on).
|
Example
|
This code fragment toggles the value of a check box.
Sub Main()
If DlgValue("MyCheckBox") = 1 Then
DlgValue "MyCheckBox",0
Else
DlgValue "MyCheckBox",1
End If
End Sub
|
See Also
|
DlgControlId (function); DlgEnable (function); DlgEnable (statement); DlgFocus (function); DlgFocus (statement); DlgListBoxArray (function); DlgListBoxArray (statement); DlgSetPicture (statement); DlgText (statement); DlgText$ (function); DlgValue (function); DlgVisible (statement); DlgVisible (function).
|