Description
|
Boolean constant whose value is False.
|
Comments
|
Used in conditionals and
Boolean
expressions.
|
Example
|
This example assigns False to a, performs some equivalent operations, and displays a dialog box with the result. Since a is equivalent to False, and False is equivalent to 0, and by definition, a = 0, then the dialog box will display "a is False."
Sub Main()
a = False
If ((a = False) And (False Eqv 0) And (a = 0)) Then
MsgBox "a is False."
Else
MsgBox "a is True."
End If
End Sub
|
See Also
|
True (constant); Constants (topic); Boolean (data type).
|