Syntax
|
FileList
array() [,[filespec$]
[,[include_attr]
[,exclude_attr]]]
|
Description
|
Fills a
String
or
Variant
array with filenames from disk.
|
Comments
|
The
FileList
function takes the following parameters:
|
|
Parameter
|
Description
|
|
Array()
|
Either a zero- or a one-dimensioned array of strings or variants. The array can be either dynamic or fixed.
If array() is dynamic, then it will be redimensioned to exactly hold the new number of elements. If there are no elements, then the array will be redimensioned to contain no dimensions. You can use the
LBound
,
UBound
, and
ArrayDims
functions to determine the number and size of the new array's dimensions.
If the array is fixed, each array element is first erased, then the new elements are placed into the array. If there are fewer elements than will fit in the array, then the remaining elements are initialized to zero-length strings (for
String
arrays) or
Empty
(for
Variant
arrays). A runtime error results if the array is too small to hold the new elements.
|
|
Filespec$
|
String specifying which filenames are to be included in the list.
The filespec$ parameter can include wildcards, such as
*
and
?
. If this parameter is omitted, then
*
is used.
|
|
Include_attr
|
Integer specifying attributes of files you want included in the list. It can be any combination of the attributes listed below.
If this parameter is omitted, then the value
97
is used (
ebReadOnly Or ebArchive Or ebNone
).
|
|
Exclude_attr
|
Integer specifying attributes of files you want excluded from the list. It can be any combination of the attributes listed below.
If this parameter is omitted, then the value 18 is used (
ebHidden Or ebDirectory
). In other words, hidden files and subdirectories are excluded from the list.
|
|
Wildcards
The * character matches any sequence of zero or more characters, whereas the ? character matches any single character. Multiple *'s and ?'s can appear within the expression to form complete searching patterns. The following table shows some examples:
|
|
This Pattern
|
Matches These Files
|
Douesn't Match These Files
|
|
*S*.TXT
|
SAMPLE.TXT
GOOSE.TXT
SAMS.TXT
|
SAMPLE
SAMPLE.DAT
|
|
C*T.TXT
|
CAT.TXT
|
CAP.TXT
ACATS.TXT
|
|
C*T
|
CAT
CAP.TXT
|
CAT.DOC
|
|
C?T
|
CAT
CUT
|
CAT.TXT
CAPIT
CT
|
|
*
|
(All files)
|
|
|
File Attributes
These numbers can be any combination of the following:
|
|
Constant
|
Value
|
Includes
|
|
EbNormal
|
0
|
Read-only, archive, subdir, none
|
|
EbReadOnly
|
1
|
Read-only files
|
|
EbHidden
|
2
|
Hidden files
|
|
EbSystem
|
4
|
System files
|
|
EbVolume
|
8
|
Volume label
|
|
EbDirectory
|
16
|
DOS subdirectories
|
|
EbArchive
|
32
|
Files that have changed since the last backup
|
|
EbNone
|
64
|
Files with no attributes
|
Example
|
This example fills an array a with the directory of the current drive for all files that have normal or no attributes and excludes those with system attributes. The dialog box displays four filenames from the array.
Const crlf = Chr$(13) + Chr$(10)
Sub Main()
Dim a$()
FileList a$,"*.*",(ebNormal + ebNone),ebSystem
If ArrayDims(a$) > 0 Then
r = SelectBox("FileList","The files you filtered are:",a$)
Else
MsgBox "No files found."
End If
End Sub
|
See Also
|
FileDirs (statement); Dir, Dir$ (functions).
|