Syntax
|
Fix
(number)
|
Description
|
Returns the integer part of number.
|
Comments
|
This function returns the integer part of the given value by removing the fractional part. The sign is preserved.
The
Fix
function returns the same type as number, with the following exceptions:
|
|
- If number is
Empty
, then an
Integer
variant of value 0 is returned.
- If number is a
String
, then a
Double
variant is returned.
- If number contains no valid data, then a
Null
variant is returned.
|
Example
|
This example returns the fixed part of a number and assigns it to b, then displays the result in a dialog box.
Sub Main()
a# = -19923.45
b% = Fix(a#)
MsgBox "The fixed portion of -19923.45 is: " & b%
End Sub
|
See Also
|
Int (function); CInt (function).
|