Syntax
|
expression1
\
expression2
|
Description
|
Returns the integer division of expression1 and expression2.
|
Comments
|
Before the integer division is performed, each expression is converted to the data type of the most precise expression. If the type of the expressions is either
Single, Double,
Date
,
or
Currency
, then each is rounded to
Long
.
If either expression is a
Variant
, then the following additional rules apply:
- If either expression is
Null
, then the result is
Null
.
-
Empty
is treated as an
Integer
of value
0
.
|
Example
|
This example assigns the quotient of two literals to a variable and displays the result.
Sub Main()
s% = 100.99 \ 2.6
MsgBox "Integer division of 100.99\2.6 is: " & s%
End Sub
|
See Also
|
/ (operator); Operator Precedence (Topic)
|