Point.GetNext (method)
Syntax | Point.GetNext |
Description | To wait for and get the next value of the point. This method returns when a point update is received for the point, based on a previously submitted OnChange , OnAlarm , OnTimed or OnAlarmAck call. If the point never changes, the call never returns. To wait with a timeout, see the GetNext (function.) |
Example |
|
See Also | Point.OnChange (method); Point.OnAlarm (method); Point.OnTimed (method); Point.OnAlarmAck (method).. |