Point.GetTimeStampHR (method)
Syntax |
Point.GetTimeStampHR param1,param2
|
|
Description | Date. To retrieve the Microsecond timestamp into 2 double 32-bit values. The timestamp indicates the time at which the point's value was read from the PLC. | |
Param1 | Double. High value of the time | |
Param2 | Double. Low value of the time. | |
Example |
|
|
See also | Point.QuadValueAsString (property, read), Point.QuadValueAsString (property, write,) Point.SetQuadIntValue (function), Point.TimeStampHR (property, read), GetTimeComponentsHR (function), GetCurTimeHR (function). |