Point (object)
Overview | The Point object provides an object-oriented interface to CIMPLICITY real-time point data. Through the object, you may set and read point values. Methods are supplied to receive the point value as it changes, periodically, or when the alarm state changes. | |
Example | 1 |
|
2 |
|
|
|
||
Notes | In the above example, a point object is created two different ways. | |
1 | Uses a new keyword; this is typically the method you will use. This constructs a point object, at which time you can set the ID of the point and use it. | |
2 | Creates a reference to a point and sets it to empty. | |
A runtime error will occur if you attempt to access methods of the object, since it is currently unassigned.
You can assign the reference to a particular object by using the SET command.
In general, you will use this with the
PointGetNext
function, which takes a list of point objects and returns the first one that changes.
Important: Point objects in
.NET scripting must be explicitly disposed of by doing either of the following:
|