Syntax
|
Point.RawValue
[
(
index
)
]
|
Description
|
Same as
Point.Value
except bypasses Engineering Units conversion if configured for the point. Will return into any type subject to some restrictions. All numeric types may be returned into any other numeric type and into string types. String and BitString types can only be returned into string types. If the variable being returned into does not have a type, the variable will be changed to the appropriate type, based on the point type.
|
Comments
|
The
option base
determines if the first element of an array point will be zero or one. If you do not explicitly set the
option base
, all arrays in Basic start at 0. If you set it to 1, all arrays in Basic start at 1. See the example below. .RawValue does not return the underlying numerical value for an enumerated point. If you want to obtain the underlying numerical value.
- Define a point with the .ID field set to
<point_id>.$RAW_VALUE .
- Reference the
.value field of this point.
|
|
Parameter
|
Description
|
|
index
|
Integer. (optional) The array element to access. Range depends on the
option base
setting.
|
Example 1
|
' Increment the points raw value by one.
sub main()
Dim MyPoint as new Point ' Declare the point object
MyPoint.Id = "TANK_LEVEL" ' Set the Id
MyPoint.Get ' Read the point
x = MyPoint.RawValue ' Return the raw value
MyPoint.RawValue = x + 1 ' Set the raw value
MyPoint.Set ' Write the value.
End sub
' Find the maximum raw value in the array.
Option base 1 ' Arrays start at one.
Sub main()
Dim MyPoint as new Point ' Declare point object
MyPoint.Id = "ARRAY_POINT" ' Set the Point Id
MyPoint.Get ' Get the value of the point
max = MyPoint.RawValue(1) ' Get first value (option base = 1)
for I = 2 to MyPoint.Elements ' Loop through all elements
if MyPoint.RawValue(I) > max then max = MyPoint.RawValue(I)
next I
end sub
' Set all elements of the array to 10
option base 0 ' Arrays start at 0 (default)
sub main()
Dim MyPoint as new Point ' Declare the object
MyPoint.Id = "ARRAY_POINT" ' Set the Id
' Loop through all elements. Since arrays are set to start
' at 0, the index of the last element is one less than the
' count of the elements.
for I = 0 to MyPoint.Elements - 1
MyPoint.RawValue(I) = 10 ' Set the raw value
next I
' Values are not written to CIMPLICITY until this
' set is executed.
MyPoint.Set ' Write the point
end sub
|
Example 2
|
'Access both the enumerated text and the underlying numerical 'value for a point.
Sub Main()
Dim p1 As New point
Dim p2 As New point
'get the enumerated value
p1.id = "ENUMERATEDPOINT"
p1.get
trace "enumerated text for " & p1.id & " is " & p1.value
'get the underlying numerical value
p2.id = "ENUMERATEDPOINT.$RAW_VALUE"
p2.get
'yes, we really mean p1.id, with p2.value!!!
trace "underlying numeric value for " & p1.id & " Is " & p2.value
End Sub
|
Note
|
Point.Value (property, read/write)
|