Syntax
|
Point.Set
[downloadPassword]
|
Description
|
To write the point's value out to the CIMPLICITY project.
An optional download password can be supplied.
|
Comments
|
The values set into the Point using the Value, RawValue , SetArray and SetRawArray methods are not written out to the CIMPLICITY project until they are committed with a Set statement.
|
|
Parameter
|
Description
|
|
downloadPassword
|
String. (optional) The download password for the project.
|
Example
|
sub main()
Dim MyPoint as new Point ' Declare the point object
MyPoint.Id = "TANK_LEVEL" ' Set the Id
MyPoint.Value = 10 ' Set the value
MyPoint.Set ' Write the value out to CIMPLICITY
end sub
|
See Also
|
Point.SetValue (property, read), PointSet (method)
|
Note
|
|