Syntax
|
Point.Value
[
(
index
)
]
|
Description
|
To retrieve or set the value in the point object. The optional index may be supplied to access values of an array point. The first element of the array is at the zero index. The value property uses Engineering Units conversion if supplied by the point. To bypass Engineering Units conversion, use the
RawValue
property.
|
|
Automatic conversion will be performed between data types as needed. The only exceptions are String and BitString points, which can only be assigned from Strings.
|
Example
|
' This subroutine show automatic type conversion
sub main()
Dim MyPoint as new Point 'Declare the point object
MyPoint.Id = "INTEGER_POINT" 'Set the Id, Point Type is INTEGER
' The string value of "10" is automatically converted to a integer
' value of 10 and place in point object.
MyPoint.Value = "10"
MyPoint.Set ' Write the point
' The floating point value of 10.01 is truncated to 10 and place
' in the point
MyPoint.Value = 10.01
MyPoint.Set ' Write the point
end sub
|
See also
|
Point.RawValue (property, read/write); Point.GetArray (method); Point.GetRawArray (method).
|
Notes
|
- To retrieve the point value, the Point.Get method must be invoked first. Once the value has been read, it can be accessed many times without having to retrieve it from the Point Manager on each reference. If the point hasn't been read, an exception is generated.
- When setting a value, the value is not written to the device until the
Set
method is invoked.
|