Program Editor Toolbars and Status Bar
The Program Editor contains the following toolbars.
Toolbar | Window | |
Standard | Main | |
Tool | Main | |
Application | Script | |
Status bar | Main |
Standard Toolbar

1 | New | Create a new document. |
2 | Open | Open an existing document |
3 | Save | Save the active document |
4 | Save All | Save all the open files |
5 | Cut | Cut the selection and put it on the Clipboard |
6 | Copy | Copy the selection and put it on the Clipboard |
7 | Paste | Insert Clipboard contents |
8 | Cascade Windows | Arrange windows so they overlap |
9 | Tile Horizontally | Arrange windows as non-overlapping tiles |
10 | Tile Vertically | Arrange windows as non-overlapping tiles |
11 | Print the active document | |
12 | About | Display program information, version number, and copyright |
13 | Dynamic | Toggle Dynamic Configuration |
Tools Toolbar

1 | Browse Point | Browse for Points |
2 | Edit Point | Edit Point ID |
3 | New Point | Create a new Point |
4 | Get Point | Get Point Value |
5 | Set Point | Set a Point |
6 | Dim Point | Dimension a Point Object |
7 | Gen Alarm | Generate an Alarm |
8 | Update Alarm | Update an Alarm |
9 | Log Status | Log a status message |
Application Toolbar

1 | Start | Start or continue execution |
2 | Break | Interrupt execution |
3 | End | End execution |
4 | Compile | Compile the document |
5 | Toggle Breakpoint | Set or clear a breakpoint |
6 | QuickWatch | QuickWatch a variable |
7 | Add Watch | Add a watch to a variable |
8 | Call Stack | Display call stack |
9 | Step Into | Step into the current line |
10 | Step | Step over the current line |
11 | Modify | Modify the value of a variable |
12 | Toggle Trace | Enable/Disable Tracing |
13 | Clear Trace | Clear the contents of the trace window |
14 | Command Line | Set the command line for the script |
Status bar

1 | Ln | Line in the script that the insertion point is on |
2 | Col | Column in the script that the insertion point is in |
3 | Pause | Script run/pause/stop status |
4 | Compiled | Displays if the script does not need to be compiled. |
5 | READ | Displays if the script is read-only. |