Syntax
|
Seek
(filenumber)
|
Description
|
Returns the position of the file pointer in a file static to the beginning of the file.
|
Comments
|
The filenumber parameter is a number that the Basic Control Engine uses to refer to the open file—the number passed to the
Open
statement.
The value returned depends on the mode in which the file was opened:
|
|
File Mode
|
Returns
|
|
Input
|
Byte position for the next read.
|
|
Output
|
Byte position for the next write.
|
|
Append
|
Byte position for the next write.
|
|
Random
|
Number of the next record to be written or read.
|
|
Binary
|
Byte position for the next read or write.
|
|
The value returned is a
Long
between 1 and 2147483647, where the first byte (or first record) in the file is 1.
|
Example
|
This example opens a file for random write, then writes ten records into the file using the PUT statement. The file position is displayed using the Seek Function, and the file is closed.
Sub Main()
Open "test.dat" For Random Access Write As #1
For x = 1 To 10
r% = x * 10
Put #1,x,r%
Next x
y = Seek(1)
MsgBox "The current file position is: " & y
Close
End Sub
|
See Also
|
Seek (statement); Loc (function).
|