Syntax
|
String[$]
(number,[CharCode | text$])
|
Description
|
Returns a string of length number consisting of a repetition of the specified filler character.
|
Comments
|
String$
returns a
String
, whereas
String
returns a
String
variant.
These functions take the following parameters:
|
|
Parameter
|
Description
|
|
number
|
Integer specifying the number of repetitions.
|
|
CharCode
|
Integer specifying the character code to be used as the filler character. If CharCode is greater than 255 (the largest character value), then the Basic Control Engine converts it to a valid character using the following formula:
CharCode Mod 256
|
|
text$
|
Any String expression, the first character of which is used as the filler character.
|
Example
|
This example uses the String function to create a line of "=" signs the length of another string and then displays the character string underlined with the generated string.
Const crlf = Chr$(13) + Chr$(10)
Sub Main()
a$ = "This string will appear underlined."
b$ = String(Len(a$),"_")
MsgBox a$ & crlf & b$
End Sub
|
See Also
|
Space, Space$ (functions).
|