About APPLICOM Communications
The APPLICOM Communications enabler uses APPLICOM Communication Server hardware and software to communicate with a variety of devices from different vendors using appropriate protocols.

Using this enabler, CIMPLICITY software can:
Poll points at a user-defined scan rate, on demand, or once at startup
- Read and write single points
- Read arrays
- Perform Engineering Unit conversion for meaningful point value displays
- Issue alarms to users when a device goes down
- Access the APPLICOM interface database
This enabler can support up to 8 APPLICOM interface cards in one computer.
This enabler supports the following CIMPLICITY features:
- Polled read at user defined rates
- Poll after setpoint
- Triggered reads
- Analog deadband
- Alarm on communications failure
- Server redundancy configuration
This enabler supports the following data types:
- Signed 8, 16, and 32 bit integers
- Unsigned 8, 16, and 32 bit integers
- Floating point
- Text
- Arrays