About Smarteye Electronic Assembly Communications
The Smarteye Electronic Assembly (SEA) Communications enabler uses the computer's serial port to communicate with Smarteye Electronic Assemblies on a multi-drop RS-232 or RS-422 network.

Using this option, CIMPLICITY software can:
- Poll points at a user-defined scan rate
- Read and write single points
- Issue alarms to users when a device goes down or a reader error occurs
- Monitor reader calibration
This enabler can:
- Support up to thirty-two (32) SEAs per serial port.
- Support up to eight (8) Smarteye readers per SEA.
- Support Polled, Handshake, and Open Loop modes of the SEA.
This enabler supports the following CIMPLICITY features:
- Polled read at user defined rates
- Poll after setpoint
- Triggered reads
- Unsolicited data (only in RS-232 point-to-point configurations)
- Alarm on communications failure
- Server Redundancy configurations
This enabler supports the following data types:
- Signed 8, 16, and 32 bit integers
- Unsigned 8, 16, and 32 bit integers
- Floating point
- Text
- Arrays