About the CIMPLICITY OPC UA Client
CIMPLICITY OPC UA (OPC Unified Architecture) Client is a device communications module that can connect to OPC UA Servers and collect data from UA Variables.
OPC UA is a standard that is rapidly gaining acceptance among vendors of process automation products in response to the complexities of inter-operability among industrial control vendors. Developed by the OPC Foundation and meant to be platform independent, OPC UA can provide lower costs and increased productivity for end-users, systems integrators and process control vendors alike by focusing communications issues on a single technology and strategy. Like CIMPLICITY®, OPC UA builds on the success and strength of common industrial standards.
OPC UA defines a platform independent communication system that has a useful and adaptive Information Model for both industrial and business application needs.
Basic components for the CIMPLICITY OPC UA Client can include the following.

1 | GE Control systems (including OPC UA Servers) |
2 | OPC UA Server connected to other control systems |
3 | Network/Internet behind a firewall |
4 | OPC UA Client |
5 | CIMPLICITY |
Note: CIMPLICITY OPC UA Client supports the basic numeric, BOOLEAN and string data types for OPC UA Data Access