APPLICOM Generic Point Addresses
The general point address format is:
<TAG><OFFSET>
Where:
< TAG > is a model-dependent prefix, which specifies the memory domain. Valid prefixes are:
Tag | Memory domain |
B | Bits |
BI | Input bits |
BO | Output bits |
O | Bytes |
OI | Input bytes |
OO | Output bytes |
W | Words |
WI | Input words |
WO | Output words |
D | Double words |
F | Floating point values |
Be aware that not all devices support all memory types.
<
OFFSET>
is the offset of the item within the domain. The generic APPLICOM device type supports the following offsets:
- Decimal addressing (radix 10)
- Address of the first element (minimum address) is 0.