CIMPLICITY Project Point Item ID Syntax

Points configured in a CIMPLICITY project are referenced for read and / or write operations using the following syntax. Each field is described below.

\\PROJECT\POINT.ATTRIBUTE

Field Description
PROJECT Required A CIMPLICITY project name under which the reference is made.
Important: When using point by address for the item IDs used by an OPC Client, the project ID must be included.
POINT Required The name of a CIMPLICITY project point.
ATTRIBUTE Required A server-defined string specifying the type of information associated with the point. A point has several attributes.