Custom Cable

The following connections are required in the cable that connects DCM and CIMPLICITY system:

There are two types of configurations for interconnecting DCM(s) to a host:

  • Point-to-point connection is between only one DCM and the host
  • A multipoint/multidrop configuration connects two or more DCMs to the host on a common line. This is a single master and series of slaves.