Default Communication Parameters
The following communication parameters are used by the OMRON communication enabler and cannot be changed. The Host Link modules in the PLC must be configured to match these settings:
Parameter | Value | Description |
Data Bits | 7 | Number of data bits used in transmissions |
Stop Bits | 2 | Number of stop bits used in transmissions |
The following communication parameters must match the Port configuration parameters for the OMRON communication enabler in CIMPLICITY software:
- Baud Rate
- Parity