Default Communication Parameters
The following communication parameters used by the CIMPLICITY Mitsubishi A-Series Serial Communication enabler cannot be changed. The A-Series Serial modules in the PLC must be configured to match these settings:
Parameter | Value | Description |
Data Bits | 7 | Number of data bits used in transmissions |
Stop Bits | 1 | Number of stop bits used in transmissions |
The following communication parameters must match the Port configuration parameters for the CIMPLICITY Mitsubishi A-Series Serial Communication enabler:
- Baud Rate
- Parity