Default Device Properties
Use the Default tab in the Device dialog box to enter information about Square D SY/MAX communications for the device. You can define the following:
Address | Each device to be accessed by the Square D SY/MAX Device Communications interface will require a sequence of one (1) or more 3-digit numbers representing the network route (for example, 100 101). |
CPU ID | Not used. |
Enable | Select Yes to enable the device when the project starts. If you select No, the device will not be enabled and points associated with the device will be unavailable. |