Default Protocol Parameters
Certain protocol parameters used by the OMRON communications enabler have been preset. They are:
Parameter | Value | Description |
DN2 | 0 | Unit Address - 0 indicates the programmable controller's CPU. This is not the same as the unit number (that is, node number) which is configurable. |
SNA, SA1 | 0,0 | Source of local network and node number. |
SA2 | FE | Source of communication unit |
SID | FF | Service ID. |