General Device Properties

Use the General tab in the Device dialog box to enter general information for the device. You can define the following:

Port Select the port for this device. Click buttons to the Port field to select the port as follows.
Display the list of ports and select one.
Create a new port, edit the current port, or select a port from the list of ports.
Description Enter an optional description to help you identify the device.
Resource Enter a resource that can be associated with this device for alarm generation. Click buttons to the right of the Resource field to select the resource, as follows.
Display the list of resources and select one.
Create a new resource, edit the current resource, or select a resource from the list of resources.
Model Type Select the type of device. Click the drop-down button to the right of the input field to display your choices, then make a selection. For this protocol, the only choice is:
SY/MAX SY/MAX-300 SY/MAX-400 SY/MAX-500 SY/MAX-600 SY/MAX-AS42C