Level Set Point Security
You can enable level set point security as follows:
- From the Settings tab on the Project Properties dialog box, highlight Points, and click Settings.
The Point Setup dialog box appears.
- Select the "Enable level set point security" check box.
If this is set, the logged-in user has only write access to those points with a level less than or equal to the level of the user. The level of the user is determined by the role that is assigned in the security section of the CIMPLICITY project.
If the "Enable level set point security" option is not selected, then all users will retain equal write access (neglecting other security options such as resource set point security).