Resource Set Point Security
You can enable level set point security as follows:
- From the Settings tab on the Project Properties dialog box, highlight Points, and click Settings.
The Point Setup dialog box appears.
- Select the "Enable resource set point security" check box.
If this option is checked, users will only have write access on points with a resource that is also in their view. A point's resource is determined in its properties. Resources in a user's view can be configured from the user's properties or from the resource's properties.
If the "Enable resource set point security" option is not selected, then all users will retain equal write access (neglecting other security options such as level set point security).