Port Configuration
When you configure a new port for APPLICOM communications, enter the following information in the New Port dialog box:
1. In the Protocol field, select APPLICOM from the list of protocols.
2. In the Port field, select the communication port that will be used for APPLICOM communications.
When you click OK to create the port, the Port Properties dialog box for the protocol opens.