Read Request Timeout

The following global parameter is used to override the default timeout setting of 5 seconds. This global parameter can be set on a project or port basis. 

The following global parameters are available to set read requests.

MBETH_READ_REQUEST_TIMEOUT
<PORT>_READ_REQUEST_TIMEOUT

MBETH_REQ_TIMEOUT

For Project
Purpose To override the project's default timeout setting.
Value n (where n is a number greater than or equal to zero)
Default Value 5

<PORT> _REQ_TIMEOUT

Where <PORT> is the name of the port.

For Port
Purpose To override the port's default timeout setting.
Value n (where n is a number greater than or equal to zero)
Default Value 5