Register Memory Addressing
Registers are 16 bit words. You can configure Analog or Boolean point types to read registers.
- For Analog point types, enter the address in the Address field. For example, R10 specifies Register 10.
- For Boolean point types, enter the register number in the Address field and the bit offset (from 0 to 15) in the Address Offset field. For example, an address of R25 with an address offset of 0 specifies the first bit in Register 25, while an address of R25 and an address offset of 4 specifies the fifth bit in Register 25.