Status Log Entries
A typical Status Log entry looks like:

The following fields have special meaning for Smarteye reader errors
Process | The port used to communicate with the reader |
Code | The error code returned by the Smarteye Electronic Assembly. Refer to the Smarteye Electronic Assembly User Manual for help in interpreting this code. |
This same code appears in a NUM format error point configured for the reader. | |
Reference | The octal address of the Smarteye reader. The first two digits indicate the Smarteye Electronic Assembly, and the last digit is the reader number on that SEA. For example, a reference of 245 would indicate an error on reader 5 of the SEA at address 240. |
Error Message | This is the message that appears in a STR format error point configured for the reader. |