Supported OMRON Devices
The OMRON C-Series and CV-Series device communication enabler supports communications to the following programmable controllers:
Communications via C-mode Host Link | |||
C20
|
C120/C500
|
CxxK
|
C2000
|
C200H
|
C1000H
|
C2000H
|
CQM1
|
C200HS
|
CPM1
|
C200HX
|
C200HG
|
C200HE
|
|||
Communications via CV-mode Host Link | |||
CV500
|
CVM1-CPU01-E
|
||
CVM1-CPU11-E
|
CVM1-CPU21-E
|
CV1000
|
CV2000
|
The following C-Series programmable controllers are supported when connected to a subnetwork, that is through a CV bridge, with FINS commands:
- C200H-CPU11-E (requires use of C200HSLK11/SLK21-V1 SYSMAC LINK Unit)
- C1000H-CPU01-EV1 (requires use of C1000H-SLK11/SLK21-V1 SYSMAC LINK Unit)
- C2000-CPU-EV1 (requires use of C1000H-SLK11/SLK21-V1 SYSMAC LINK Unit).
When configuring communications to programmable controllers on subnetworks, you must ensure that the programmable controllers attached to the Host Link is configured with the proper routing tables to reach the desired programmable controllers on the subnetworks. Refer to the OMRON documentation for details on setting up these routing tables.