Timeout Retry Delay
The following global parameter is used to set the length of time, in ticks (i.e. 0.01 seconds per tick), to pause when a read request fails before sending the request again. This global parameter can be set on a project or port basis.
The following global parameters are available to set timeout retry delays.
MBETH_TIMEOUT_RETRY_DELAY |
<PORT>_TIMEOUT_RETRY_DELAY |
MBETH_
TIMEOUT_RETRY_DELAY
For | Project |
Purpose | To set the length of time, in ticks, to pause when a read request fails before sending the request again. |
Value | n (where n is a number greater than or equal to zero) |
Default Value | 0 |
<PORT>
_
TIMEOUT_RETRY_DELAY
Where <PORT> is the name of the port.
For | Port |
Purpose | To set the length of time, in ticks, to pause when a read request fails before sending the request again. |
Value | n (where n is a number greater than or equal to zero) |
Default Value | 0 |