Types of Modbus RTU Slave Configuration Records
The configuration file may contain the following types of records:
IP address Parameters | Defines the serial communications port and settings. | |
Trace Log Parameters | Specifies state (on/off) of protocol stack diagnostics logging. | |
Modbus Register Limits | Defines the range of valid values for a Modbus analog register (memory type 3X or 4X). | |
Register Mapping | Defines a mapping between a CIMPLICITY point and a Modbus data address. | |
Comments | Any line beginning with one or more pound signs (#). Ignored by the Modbus RTU Slave Interface. | |
Blank lines | Ignored by the Modbus RTU Slave Interface. |