Viewing an Antenna's Current Configuration
You can configure Diagnostic Points for each antenna in your CIMPLICITY project to display an antenna's current configuration values.
Diagnostic Points are configured the same as any other device point, except that a special address value is used, and the Diagnostic Data checkbox is selected. The four special addresses you will use to create these Diagnostic Points are:
Configuration Value | Point Address | Point Type |
Tag Type | $TAG_TYPE | USINT |
Object Detect Mode | $OBJECT_DETECT_MODE | USINT |
Object Detect Timeout | $OBJECT_DETECT_TIMEOUT | UINT |
RF Field Strength | $RF_FIELD_STRENGTH | USINT |