Change a Port's Protocol
About this task
In your CIMPLICITY project configuration, device and point data are protocol dependent. You cannot delete a port then re-add it using another protocol if device and point data for the original port still exist.
todo: To change a port's protocol:
Procedure
- Export the point data for the port using the Import/Export utility if you plan to re-use the same point data.
- Delete the point data for the port.
- Delete the device data for the port.
- Delete the port.
- Create the port with the new protocol.
- Define the devices for the port.
- If you exported the point data, then use the Import/Export utility to import the point data. Otherwise, define new points.