Modbus RTU Port Configuration

Procedure

  1. In the Protocol field, select MODBUS RTU from the list of available protocols.
  2. In the Port field, select the communication port that will be used for Modbus RTU communications.

    When you click OK to create the port, the Port Properties dialog box for the protocol opens.