OPC Server Data Storage
About this task
Note:
Open the OPC Server window at least one time before allowing clients to attach to the OPC Server.
Because of a change in how OPC Server data is stored beginning with CIMPLICITY 7.0, opening the OPC Server enables you to determine if legacy project/log in data was read from the Registry or if you need to add projects to the OPC Server configuration.
By opening the OPC Server at least one time, you are either:
- Enabling the OPC Server to perform a configuration upgrade, provided there is registry based configuration from a previous OPC server version.
- Doing a first time configuration, if no registry configuration was found.