Important: You do not have the latest version of CIMPLICITY! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the CIMPLICITY product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GE Digital Sales Support. For the most up-to-date documentation, go here.
Configure a Self-Signed Certificate
About this task
After starting the OPC UA Security Configuration from the CIMPLICITY Workbench, the CIMPLICITY OPC UA Certificate Configuration dialog box appears.
The elements in this dialog box are described in the following table:
Field
Description
Use GDS
This check box is selected by default. For a self-signed certificate, clear this check box.
For a GDS Certificate, leave this check box selected.
Enable Security
This button sets up secure OPC UA communications using certificates. The CIMPLICITY serverconfig.xml file location is displayed next to this button.
Display area
Shows the progress and displays the results when the Enable Security button is clicked.
Check Status
When using GDS, click to check the status of pending requests.
Advanced
This button opens another screen to view and select configuration options.
Redundancy Selection Box
Used to specify whether you are configuring the certification for the primary or secondary node. This option is available only for projects with Server Redundancy enabled.
Clear Trust List
This check box allows you to clear the current Trust List. If unchecked, the GDS-assigned Trust List is added to the existing Trust List.
Toggle Log
Used to toggle the Configuration Log window on and off.
Close
Closes this page.
Self-signed Certificate Configuration
Do the following.
1
Clear the Use GDS checkbox.
2
Click Enable Security.
Result: A self-signed certificate that can be used by the CIMPLICITY OPC UA Client is created.
Advanced Configuration
Procedure
Click Advanced to see more detailed information about the certificate settings and to directly select or create specific certificate instances.
A Self Signed Certificate Configuration Form opens enabling you to do the following.